5/11/2015 12:03 PM | |
Posts: 3 Rating: (0) |
I have touch panel TP170b , اكتب نصًا أو عنوان موقع ويب أو ترجم مستندًا. The program has been uploaded(backup) because there is no memory card and I can not contact the supplier and machine is old , and this type of panel is obsolete, if I buy a new version the program will not downloaded is there any solution to convert the program ---------------------------------------------------------------------------------------------------- Split from problem in simatic touch Panel. |
Last edited by: Min_Moderator at: 5/11/2015 3:02:32 PMNew subject after splitting |
|
5/11/2015 8:53 PM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello, sorry either you have a original program or you have to buy the same panel with the same part number. |
1/22/2016 3:34 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
New question published by Jon CCEE is split to a separate thread with the subject Load a program from a TP170B onto a TP177B and operate as per the original HMI. Best regards |