9/20/2011 9:36 AM | |
Posts: 3 Rating: (0) |
Hello! Yes, I have the same problem with the HMI. This type of HMI:TP177B 6" COLOR PN/DP. The network type:Profibus |
9/20/2011 9:39 AM | |
Posts: 3 Rating: (0) |
Hello! Yes, I have the same problem with HMI. This type of HMI: TP177B 6" PN/DP. The network: Profibus Landras |
9/20/2011 9:53 AM | |
Joined: 1/17/2007 Last visit: 10/6/2020 Posts: 289 Rating: (3) |
I already send the devices to Siemens repair service for more diagnostic. I will keep you in touch. |
9/21/2011 8:00 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181)
|
Hello Amit, To be honest I don't know what to suggest you. I have almost the same behavior with OP77. But that is happening after problems in our power supply substation. After a few restarting panel is going healthy. Better observe all the conditions there at the moment when that behavior happens. If you have on hands another panel (new one), you could replace it in order to see if that behavior will repeat again. If yes, means both panels are OK - the problem is outside. Try it with Support Request as suggested above. Best regards, Hristo Mihalev |
This contribution was helpful to1 thankful Users |
10/18/2011 11:30 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181)
|
Did you receive any info from Siemens about the way of solved the problem? Best regards, Hristo Mihalev |
Follow us on