11/8/2017 6:53 AM | |
Joined: 10/7/2005 Last visit: 2/18/2025 Posts: 3037 Rating:
|
Hello SimaticBob
well, there sort of is, but I'm not too sure if you like it. Anyhow, the TP1900 does support Modbus Master protocol, so you could add a CP341 with Modbus Slave driver and connect your TP that way. If you have no space left in your ETM200M rack and fear the cost of another ET200M with CP341 card and Modbus driver, you can also use an ET200S(P) with a 1SI card instead (which is what our good friend Navnag did ages ago and proved to work, see THIS thread for more). Other (non Y-Link related) alternatives are as per general Siemens guideline on How to connect HMI panels to a H System (based on WinCC flexible HMI, but concepts should equally apply to TIA Portal HMI). |
Cheers |
|
11/8/2017 12:37 PM | |
Posts: 1 Rating:
|
Thanks ! Will look into your suggestions |
Follow us on