7/14/2017 9:43 AM | |
Joined: 8/3/2009 Last visit: 4/25/2025 Posts: 15355 Rating:
|
Hello I´m not sure if I understand your Usecase in the right way... do you want to export your Data logs that is running in the Panels Runtime into a csv file with a PLC Bit as trigger? Then you can use the following FAQ for copying the Log: https://support.industry.siemens.com/cs/ww/en/view/63042926 And for the Trigger use the PLC Tag with the Aquisition Mode "cyclic continous" and use the Event "Value Change". -> The Value Change Event runs every time you get a rising AND a falling Edge on that bit, so so a toogle instead of just set the Bit to HIgh. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on