11/2/2024 3:57 PM | |
Joined: 1/8/2022 Last visit: 2/21/2025 Posts: 1 Rating:
|
Hello, I have the same problem as colleagues before me: The same panel is in HWconfig. the correct firnware (15.0.0). I've installed the latest panel images (TIA17u8). Everything in the HW config is the same as the device. Still i'm receiving the message: download has failed due to missing panel image. and warning: the target (...) in the offline project is different from the target (...) in the online project latest panel image update. HWconfig and device are the same. and this problem is the same on 6 touch panels that I'm working with. Any help is welcome (and needed heh) thanks <3 ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 11/04/2024 09:04:18New subject after splitting |
|
Follow us on