1/25/2018 12:37 PM | |
Joined: 5/12/2006 Last visit: 4/24/2025 Posts: 22624 Rating:
|
hello, yes is the same. On the HMI PC the RT Loader allows the TransferOption on the PC HMI.
Christoph |
1/29/2018 12:23 PM | |
Joined: 8/3/2009 Last visit: 4/25/2025 Posts: 15350 Rating:
|
Hello qwemx If you want to be sure that you know all options, you can also do an offline transfer like this (if you have any problems ...): until V13: https://support.industry.siemens.com/cs/ww/en/view/103198851 With V14 or later: https://support.industry.siemens.com/cs/de/en/view/109740696 hope it helps Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on