12/24/2022 4:14 PM | |
Joined: 3/28/2015 Last visit: 4/19/2024 Posts: 721 Rating: (213) |
Hello,
No Restore the backup to the same panel type only. You should have the configuration program for ''KTP600'' and in this case you change the panel type into''KTP700'' |
Eng.Mohamed Ibrahim |
|
12/26/2022 4:32 AM | |
Joined: 3/28/2015 Last visit: 4/19/2024 Posts: 721 Rating: (213) |
Hello, The backup taken via USB is not open or edit but it restore to the same panel type only. If you have the configuration program''application''you can open it with WinCC TIA and right click on the HMI''KTP600''-->select replace the panel-->select ''KTP700''then compile and save, after that you can download the program to''KTP700'' |
Eng.Mohamed Ibrahim |
|
Follow us on