11/23/2020 9:46 PM | |
Joined: 2/6/2015 Last visit: 4/4/2025 Posts: 80 Rating:
|
Hi KEMP_ARVE, With a KTP600 Basic Color DP you should use a PC Adapter USB A2 (6GK1 571-0BA00-0AA0). Look at this FAQ: Which connector cables are available for connecting to SIMATIC Panels? Best Regards, CGA81 |
If this Information really helps, you could use the Rate function |
|
11/23/2020 10:04 PM | |
Posts: 2 Rating:
|
So there's no way to transfer to the panel through the module by using an ethernet connection with the CPU? |
11/24/2020 8:29 AM | |
Joined: 4/24/2006 Last visit: 4/18/2025 Posts: 8956 Rating:
|
Hello, Perhaps this link might help In WinCC (TIA Portal), how do you transfer a project to an HMI panel using S7 Routing? Best regards, Wizard |
Follow us on