Industry Online Support
Technical Forum
5/2/2008 10:19 AM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (318)
|
Hi Abdelaal, The SFC14/SFC15 are capable for that, see the help when you are standing in STEP7 in the system library on SFC14 and/or SFC15. See also: How do you read data consistently from a DP standard slave/PROFINET IO device and write it consistently to a DP standard slave/PROFINET IO device? |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on