6/14/2014 6:05 PM | |
Posts: 8946 Rating:
|
Mostly, USB adaptor is "simulating" a RS232, so please try the RS232/PPI Muli-Master cable selection. Also, this link may be helpfully: http://support.automation.siemens.com/WW/view/en/22809353 |
Last edited by: IBN-Service at: 6/14/2014 6:26 PMLink http://support.automation.siemens.com/WW/view/en/22809353 |
|
This contribution was helpful to
1 thankful Users |
6/14/2014 6:47 PM | |
Joined: 1/21/2013 Last visit: 11/20/2024 Posts: 4620 Rating:
|
Hello R&H CO. and How can you transfer a WinCC flexible project - Siemens Industry ... and Can USB PC adapter (6ES7972-0CB20-0XA0), be used in transfering ... |
This contribution was helpful to
1 thankful Users |
6/15/2014 9:47 AM | |
Joined: 5/28/2008 Last visit: 2/12/2025 Posts: 4518 Rating:
|
Hello, Attached a large matrix with all possible connection to most of Simatic Panels. Go for MP277 and see the possible connection. Please note that it is marked in MPI that it is possible and note that it's not possible with PC adapter (6ES7 972-0CB20-0XA0). I mean it is not possible to connect between your PC and Panel using PC adapter. But you can use MPI port of your PC (if applicable) to transfer proect to MPI port of your Panel. And you can use PC adapter in what we call "S7-routing" by connecting it between PC & CPU. And cnnect your Panel to CPU and transfer to the panel -through CPU- using S7-routing feature as per the following link: Hope this helps.
AttachmentProjekttransfer_e_C1.pdf (89 Downloads) |
Ayman Elotaify |
|
6/20/2014 11:04 AM | |
Posts: 67 Rating:
|
thanks Ayman i use Ethernet cable and i think it`s very usefull and fast more than PC/PPI cable ... |
This contribution was helpful to
1 thankful Users |
Follow us on