10/5/2016 9:14 AM | |
Joined: 8/25/2014 Last visit: 4/16/2025 Posts: 133 Rating:
|
Hello all. I am working in TIA portal V13 sp1 update 9. I made a project that has 2 languages, my native language and the foreign language.When I completed the user interface I exported the language text of the TIA project and had it translated. The exported file had two language columns, one column for my native language which and a blank language Colum where the translator put in the translated text. Now when I want to import this translated text, nothing happens. The importing goes through without errors but the second language column in the TIA portal stays empty. Any ideas as to why the translated text doesn't show in the TIA portal? Best regards. Ales ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 10/6/2016 11:03:32 AMNew subject after splitting |
|
10/6/2016 2:29 PM | |
Joined: 2/27/2014 Last visit: 3/27/2025 Posts: 689 Rating:
|
Hello, While exporting see the source language. Select foreign anguage as source language and export in to csv file. After exporting edit/translate the native language text to foriegn languge and save it . Now import the file and do the tock mark on import source lanague. For better understanding see the attached Video. If you feel this post is useful then don't forget to rate. AttachmentLang.zip (263 Downloads) |
With Best Regards, |
|
6/28/2017 12:51 PM | |
Posts: 1 Rating:
|
Sending a video as some .exe file of unknown orgin not a good idea. VIRUS WARNING!!! |
Follow us on