1/28/2019 2:13 PM | |
Joined: 9/6/2015 Last visit: 5/7/2024 Posts: 4 Rating:
|
Hi all experts! I'm having a bit trouble with UDP communication with a CPU 1512SP-1 PN and a Kongsberg Seatex MRU 3. The MRU is set to output values in a UDP broadcast packet, IP address 192.168.0.20, subnet 255.255.255.0. PLC is set to ip 192.168.0.10, subnet 255.255.255.0. A connection is set up for the MRU, local ID 0x100, Partner is set to "(All broadcast devices)" and connection type is set to UDP connection. Program consists of a single network in OB1 with a TRCV_C FB with a separate instance DB. All inputs and outputs are to a DB (Params) for easy troubleshooting. Attached is project file and screenshots. Is there something i have overlooked in the configuration? I get error 0x809B "InterfaceID is invalid". Kind regards Lars Lone
AttachmentS7-1500_MRU.zip (91 Downloads) |
1/29/2019 2:50 PM | |
Joined: 9/6/2015 Last visit: 5/7/2024 Posts: 4 Rating:
|
Hi, thanks for all help. I managed to solve it, it was wrong parameters :) |
Follow us on