5/25/2011 6:09 AM | |
Joined: 3/21/2006 Last visit: 1/14/2025 Posts: 10239 Rating: (1182) |
Hello Jeff, If trial version of software exists, you should received it from local Siemens rep. More info about new Step7 look at TOP Links for TIA V11; STEP7 V11; WinCC V11 Best regards, Hristo Mihalev |
5/25/2011 7:56 AM | |
Joined: 5/28/2009 Last visit: 1/18/2025 Posts: 127 Rating: (10) |
Hi... umann TIA Portal V11 not for only S7-1200 its is also S7-300 & S7-400 serise . You have used only S7-1200 go for TIA Porta V10 . same view and controlavalable on this version. |
Regards, |
|
5/29/2011 4:05 PM | |
Joined: 8/16/2010 Last visit: 7/8/2024 Posts: 50 Rating: (8) |
Unless I am mistaken I think that it is not possible to download from the Siemens website, I'm not even sure if a trial version is available although I seem to recall reading somewhere that it does work for a time limited period without activation. I could be wrong though as I've not been able to find this again. Anyway, if you are interested in the Lite version then this can be found here.... http://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&objId=39596695&nodeid0=10805396&load=content&lang=en&siteid=cseus&aktprim=0&objaction=csview&extranet=standard&viewreg=WW Sorry about the rather long url. Regards, RandomCoder |
5/29/2011 4:15 PM | |
Joined: 3/21/2006 Last visit: 1/14/2025 Posts: 10239 Rating: (1182) |
Makes the difference between "Lite" and ordinary version - What are the essential differences between STEP 7 Lite and STEP 7 / STEP 7 Professional? For the moment there isnot availible v11 for download. Best regards, Hristo Mihalev |
5/29/2011 8:52 PM | |
Posts: 947 Rating: (45) |
Use of V11 - it's like to work for free beta tester . Have to wait another six months, or even better year |
Follow us on