3/19/2018 5:19 PM | |
Posts: 25 Rating: (0) |
Hello, I am replacing a S7 1200 CPU 1214C AC/DC/RLY 6ES7 214-1BE30-OXBO which is water damaged. This unit is obsolete but I have a equivalent which is the 6ES7 214-1BG40-OXBO. I have change the CPU in the program on my laptop to the 6ES7214-1BG40-OXBO Version 4.1. But the PLC is version 4.2.1 I tried to download the firmware V4.1.2 to downgrade the PLC version, but I need to be register which I have done but has not received yet a confirmation. Is there any way I can download this firmware? Thank you for your help. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/20/2018 9:04:17 AMNew subject after splitting |
|
3/20/2018 10:52 AM | |
Posts: 531 Rating: (34) |
Also keep in mind that you could always open a hotline case and ask for the download there. The hotline guys will help you with upcoming issues, too. |
3/20/2018 1:02 PM | |
Posts: 25 Rating: (0) |
Second picture |
3/20/2018 1:02 PM | |
Posts: 25 Rating: (0) |
Third picture |
3/20/2018 1:36 PM | |
Joined: 5/12/2006 Last visit: 9/25/2024 Posts: 22372 Rating: (3014) |
click on the green arrow in the message line and it opens the code line which chause the error regards christoph |
3/20/2018 2:55 PM | |
Posts: 25 Rating: (0) |
Hello Christoph, Thank you, Can you check for me this 3 Network. This is where I have the error " conversion is not supported because both data type are the same. Thank you again. AttachmentFC1 Alarm.xlsx (281 Downloads) |
3/20/2018 4:11 PM | |
Posts: 25 Rating: (0) |
Hello BR, thank you, Is it good like this? |
Follow us on