1/16/2008 7:53 PM | |
Posts: 3 Rating: (0) |
I'm trying to establish a profibus network with two 315 2DP PLC's one as a master and one as a slave. I have been using this training document as a guide However when I get to to step 31 the configuration tab appears as in the attachment.This is unlike that of the document which appears to be the same for configuring the slave (in the case of the slave the configuration tabappeared slightly differently but the same information could be inputed) Has any one any advice on what to enter into this table in order to correctly configure the master. Also if anyone is feeling generous could they explain what the different pieces of information in the configuration table mean as I don't understand what exaclty it is doing. Any help is much appreciated. |
1/16/2008 10:43 PM | |
Joined: 1/7/2006 Last visit: 12/23/2024 Posts: 2705 Rating: (320)
|
Hi, See the example DP link between CPU 315-2DP (slave) and S7-400 (master) This is a example for MS {Master-Slave} DP communication. The DX are for listening to another Slave where the iSlave can "see" also the data to the Master... |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
2/4/2008 8:39 PM | |
Posts: 3 Rating: (0) |
Thanks for the help guys I've managed to get the network set up and communicating |
Follow us on