5/22/2015 1:33 PM | |
Posts: 3 Rating:
|
hi. Im having trouble with my KTP600 and S71215. im using TIA V13, and use the HMI to edit some boolic tags in the PLC as well as retrieving a couple of registers. The issue im having is that the HMI wont edit the tags in the PLC, and it also dont retrieve the value from the registers. The wierd thing is that i have one tag that is working. In attachment is one of the events that is not working, HMI taglist, PLC taglist and the working event
Im quite new to programming in TIA, os i might have forgotten something very basic. AttachmentScreenshots.zip (54 Downloads) |
Last edited by: Min_Moderator at: 5/22/2015 3:56:53 PMMove Screenshots to attachment |
|
5/26/2015 7:09 AM | |
Posts: 1299 Rating:
|
Hello, which version of TIA portal are you using? what's the "release" event of the button that is not working? K!ke |
Follow us on