7/4/2018 10:27 PM | |
Posts: 2 Rating: (0) |
Hi Siwarexi, I am trying to execute the zeroing command, but I get this error: #6054 and #4531 That is a "Scale Command Error", because weight outside allowable zero range. I try to set this parameters: - SEMI_AUTO_ZERO_LIMIT_NEGATIVE (DR3) = 1 - SEMI_AUTO_ZERO_LIMIT_POSITIVE (DR3) = 12 But I got the same error. The actual weight is 8. To set this parameters I entered to "Service Mode" - s_CMD2: i_CMD_CODE =1 I set the values to the DR3 tags and go back to the "Service Mode Off". Is the process to send the configuration parameters correct? Best, Richard
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 7/5/2018 6:44:37 AMNew subject after splitting |
|
Follow us on