1/14/2015 2:50 PM | |
Joined: 6/12/2012 Last visit: 2/8/2024 Posts: 165 Rating: (7) |
Thanks for the input! I have attached the project. I do not have Step7 5.5 on my laptop since it can not be installed on my OS and I can not pass from IBH softec to TIA v12!
AttachmentABB_DRIV.zip (741 Downloads) |
Last edited by: Min_Moderator at: 1/14/2015 3:19 PMMove zip-file in attachment Thanks, |
|
1/14/2015 3:11 PM | |
Joined: 6/12/2012 Last visit: 2/8/2024 Posts: 165 Rating: (7) |
I'm using TIA v12 Professional. |
Thanks, |
|
1/14/2015 3:30 PM | |
Joined: 5/12/2006 Last visit: 9/24/2024 Posts: 22371 Rating: (3012) |
Hello, ic have attached the converted project from ABB. Extract it and open in in TIA then you can copy then FB's and UDT's in your TIA. Regards Christoph AttachmentD:\ABBDrive_V12.zip (758 Downloads) |
This contribution was helpful to1 thankful Users |
1/16/2015 1:27 PM | |
Joined: 6/12/2012 Last visit: 2/8/2024 Posts: 165 Rating: (7) |
Hi! Regarding this Project I have change it to the configuration in attachment. I want to give a start command to the drive. Is this configuration correct when I send it by PROFIBUS? The tags of the PZD words of the drive are correct? Thanks.
AttachmentDrive ABB.zip (598 Downloads) |
Thanks, |
|
1/16/2015 1:32 PM | |
Joined: 6/12/2012 Last visit: 2/8/2024 Posts: 165 Rating: (7) |
I am using the PPO type 6 packcage of PROFIBUS. Here is the PPO image of the drive. |
Thanks, |
|
4/13/2015 9:03 PM | |
Posts: 2 Rating: (0) |
Is it possible to convert program to TIA Portal V11 SP2 Update 5 Professional because I can't open project in V12 Version |
Follow us on