9/9/2019 7:43 AM | |
Joined: 8/12/2018 Last visit: 8/28/2023 Posts: 47 Rating:
|
Thank you, but I know that. the addresses are not clear in the previous figure, see the this figure. |
9/9/2019 9:42 AM | |
Joined: 8/12/2018 Last visit: 8/28/2023 Posts: 47 Rating:
|
Yes this is the problem, so how can I do the communication?? I cant change the hardware configuration of the project. |
9/9/2019 10:25 AM | |
Joined: 6/24/2013 Last visit: 3/21/2025 Posts: 1674 Rating:
|
you can use a software connection (not defined in connections but created in a program) 1. Create a Connection with TCON 2. use sequences to read/write 3. in case of errors invoke connection reset 4. you can use diag to capture specific errors. see attached file and block FB101 which contains a sketcho of TSEND TRCV comms implementation AttachmentETH_COMMS.zip (126 Downloads) |
Follow us on