10/17/2008 11:17 AM | |
Posts: 5822 Rating:
|
Dear Michael, maybe you try this sample project. Best regards J_Bell AttachmentS7_on_pn.zip (503 Downloads) |
6/27/2009 4:50 AM | |
Posts: 90 Rating:
|
Hi J_Bell, I have tried to work with your sample project using PLCSIM V5.4 SP3, but I amhaving problems to download the stationsusing NetPro. First allI transfered by PLCSIM(MPI) interface bothhardware (SIMATIC PN 1 and SIMATIC PN 2) to PLCSIM (S7-PLCSIM1 SIMATIC PN 1 and S7-PLCSIM2 SIMATIC PN 2) using HW Config and it was ok (picture1.JPG). The problem occursafter when I try to transferthe stations using Netpro (right click on thestation>Download>Selected Station). After transferedthe twostations by Netpro, both S7-PLCSIM CPU 1/2assume the same configuration (S7-PLCSIM1 SIMATIC PN 2 and S7PLCSIM2 SIMATIC PN2) - picture2.JPG. I have already checked and theCPU portIP adresses are differents and ok (192.168.0.1 and 192.168.0.2 as the sample project). Please, what is the correct procedure to transfer the s7-connection using Netpro without overwrite the sameconfigurations in both CPU PLCSIM ? I hope I have managed clearly myissue !! Greetings ! Attachmentpicture_1_2.zip (269 Downloads) |
6/28/2009 2:54 PM | |
Joined: 10/7/2005 Last visit: 2/19/2025 Posts: 3038 Rating:
|
Hello Denker I am unable to replicate the problem that you are having (it's working fine on my Laptop) but why don't you simply use this workaround for the time being: 1.) Save and compile HWconfig of both PLC's and NETPRO. 2.) Open up PLCSIM, select the Block folder of your first PLC and download it all to it. 3.) Open up another instance of PLCSIM anddo the same for the second PLC. Make sure that you click on YES when asked if you want to download the system data (the SDB container in the program folder of each PLC contains the compiled HWconfig and NETPRO for that PLC so this will fix the problem you have with you NETPRO download by achieving the same in a slightly differnet way). I hope this helps |
Last edited by: fritz at: 6/28/2009 2:57 PMCheers |
|
This contribution was helpful to
1 thankful Users |
Follow us on