3/7/2017 1:23 PM | |
Posts: 6 Rating:
|
Hi all, I need to link two TP1200 comfort panels to a single S7-1200 PLC running identical displays but can't work out how to do it. The ideal solution would be a single HMI project which is uploaded to both HMIs, but I guess that would cause communication problems. Failing that I'd like to clone the HMI project as suggested in this topic: https://support.industry.siemens.com/tf/WW/en/posts/one-project-on-two-hmis/138812?page=0&pageSize=10 but I can't seem to make that work in TIA portal 13 - I have the option to copy an HMI project on the right click menu, but I can't make it paste. Has anybody managed anything like this before? Many thanks, Ben. |
Last edited by: TheGribble at: 3/7/2017 1:24:21 PMLast edited by: TheGribble at: 3/7/2017 1:25:48 PM |
|
Follow us on