3/6/2014 1:42 AM | |
Joined: 10/7/2005 Last visit: 3/25/2025 Posts: 3042 Rating:
|
Hello Ebrahim_1 there's two ways you should be able to solve this: 1.) Use a seperate Ethernet port on your ibaPDA Server and connect PLC 2 to it. 2.) Routing is supported for S7 Analyzer as as of ibaPDA V6.28.0 (latest ibaPDA at time of writing is V6.31.3 and as always a free of charge download for registered iba users). For this to work, you would route through PLC1 onto PLC2 but need to obviosuly have a physical Ethernet path from PLC1 to PLC2 and configureNetpro accordingly. In the ibaPDA you then go to theI/O Manager, add a second S7 Analyzer TCP/IP connection and enter the routing information (Gateway PLC's IP address an S7 NetPro Subnet ID of target network). Note: The devicesthat you route through must support routing, so check this first and see Which modules support the S7 routing function? for more on this. I hope this helps |
Last edited by: fritz at: 3/6/2014 2:51 AMAdded S7 routing link Cheers |
|
This contribution was helpful to
1 thankful Users |
3/6/2014 10:28 PM | |
Posts: 79 Rating:
|
It helped. I will go with the first option. seems easier to do. Thanks
|
This contribution was helpful to
1 thankful Users |
Follow us on