10/16/2020 6:43 PM | |
Joined: 6/26/2019 Last visit: 9/18/2023 Posts: 22 Rating:
|
Hello, I think there is a bug in the 1.0.2 image of the IOT2050. Or there are two node-red installed. I update the node-red: cd / usr / lib npm install -g --unsafe-perm node-red https://support.industry.siemens.com/tf/WW/en/posts/upgrade-node-red/239784?page=0&pageSize=10 (I attach messages from the installation) If node-red is run at boot, the IOT2050 GPIO node is preserved but with version v1.0.2 If I run systemctl stop node-red and then manually run node-red, v1.2.1 opens, but whitout IOT2050 GPIO node. I have remounted the image and changed the /lib/systemd/system/node-red.service (see attached images) But the problem persists. Is there a way to update the node-red that runs when we select autostart on the iot2050setup?
Attachmenttwo_node_red.zip (271 Downloads) |
11/24/2020 10:33 AM | |
Joined: 4/28/2015 Last visit: 9/27/2023 Posts: 3258 Rating:
|
Hi, I have a solution for this, posted here. Best regards! |
11/27/2020 9:11 AM | |
Joined: 6/26/2019 Last visit: 9/18/2023 Posts: 22 Rating:
|
Thank you very much, it works! |
Follow us on