3/29/2012 4:04 PM | |
Joined: 1/15/2009 Last visit: 4/19/2024 Posts: 316 Rating:
|
Hi Rainery, Yes, you can use non-siemens switches, however it is my experience having them is best. Siemens will support there switches and can provide more help in their setup and diagnosing what is and what isnt a w switch problem.... but the short answer is, a non siemens switch can work. For your setup,your rack PCs through me off a bit, those are trying to represent the controllers (S7-400Hs) right? Now even though the CP443-1EX20 has two ethernet ports, you will only use one. Because you have redundant controllers, each CPU has an CP443-1, thus a redundant rack will have 2 CPU and thus 2 CP443-1s. I have created a little sketch to represent what I am describing. You also can have a connection between the two busses, if you setup your switches for a Ring Manager and a Standby (this is certain if you use Siemens switches).... My one question is, is one of the PC stations an ES/OS and the other is an OS? Thanks
Attachmentnetwork.PDF (155 Downloads) |
The best location for all PCS 7 content (manuals, guides, application notes, FAQs, and videos). |
|
This contribution was helpful to
1 thankful Users |
3/29/2012 4:47 PM | |
Joined: 4/19/2008 Last visit: 11/21/2024 Posts: 1525 Rating:
|
Hello Rainery, you can follow the Scheme Given by RugbyGuy, For the Configuration of the S7 With Fault Tolerant Connection Link. How do you configure a fault-tolerant S7 connection for a user application via Industrial Ethernet with the SIMATIC NET PC software? |
Ammy |
|
This contribution was helpful to
1 thankful Users |
3/30/2012 3:17 PM | |
Joined: 4/19/2008 Last visit: 11/21/2024 Posts: 1525 Rating:
|
Hello RugbyGuy, the Both WinCC Station are Stand alone Configuration, there is a no any Communication (link) between COM port or Ethernet. this Setting required in the Redundent Server Configuration. here both are independent & both Station are in Runtime, & there is a no any Switch over between two Station. if you used the Server Client Confiuration in that it is required which one is master & Slave, from which Server the Client PC is going to fatch the Data, is it clear for you. as you mention you required the ES, but one of the machine you can act as a ES/OS & other is only OS Station...... |
Last edited by: Ammy at: 3/30/2012 3:19 PMES Point Added. Ammy |
|
Follow us on