Industry Online Support
Technical Forum
2/11/2021 6:30 PM | |
Posts: 10 Rating:
|
Hi everyone. maybe someone will have ideas ... given: two S120 drives with one CU320, not parallel. two motors on one shaft, each with its own encoder, SMC30 encoder modules. the first drive falls off by error 31118, the second works normally. there is an opportunity to work with each drive separately and in tandem, one with speed control, the second with torque. what was checked: encoders and cables checked. screens checked. the encoders were connected from motor 1 to the second drive and from the second motor to the first drive. swapped places of SMC30. one encoder is disabled and a jumper is inserted between two SMC30s on channels A, B, Z (UTP, not the first time and on different drives, until a new encoder arrives ...). replaced by CU320. the project was uploaded from a running drive. the drive was reset to factory settings. crutches: F31118 moved to warning, P0492 raised to 500. P.S. I would like to understand the reason and get rid of the crutches ... I have no more ideas. the number of spare parts is limited. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/12/2021 08:19:55New subject after splitting |
|
Follow us on