8/29/2017 10:55 AM | |
Joined: 7/19/2017 Last visit: 10/17/2023 Posts: 64 Rating: (0) |
Hi bergmanu, i use the UART method of Mraa class in eclipse to finish the com communication . But i found some problems (the pico i used is the release one not the sample) : 1. when i use the writeStr method , the receive port will receive the string but have "!!" characters in the front of it. If i did not use writeStr method ,it also receive the "!!" character. why ? 2. when i use the ReadStr method to get the string from send port , i found if the speed is not as fast as possible it won't receive any string or only a part of string or some wrong string. why ? Does it need the special com cable , i use the siemens box or panel com port cable? Best regards,
------------------------------------------------------------------------------------------ |
Last edited by: AutoGen_5750863 at: 8/30/2017 3:06:41 AMLast edited by: The Helping Hand at: 9/7/2017 7:51:57 AMNew subject after splitting |
|