Industry Online Support
Technical Forum
5/15/2011 8:03 PM | |
Posts: 71 Rating:
|
Hi; I'm searching for UDT applications which consists of screen shot examples. Anybody has these kind of manuals thnks |
5/15/2011 9:38 PM | |
Joined: 1/28/2009 Last visit: 5/26/2023 Posts: 6802 Rating:
|
check the following link for more information How do you create and parameterize variables and the IN, OUT and IN_OUT parameters of the UDT data type? regards |
5/24/2011 8:19 AM | |
Joined: 9/6/2008 Last visit: 5/7/2022 Posts: 1121 Rating:
|
Hi Ercanbozi well please find the attached UDT example screen shot, But please not that once you have called the UDT in say FC or FB then the any change in the UDT shall affect the call in FC or FB repectively. Again if you have a do a repeat the same data type again and again then you can use UDT Note that UDT can increase the Size of the BLOCK Have fun.. AttachmentUDT_help.zip (64 Downloads) |
Jazz |
|
5/24/2011 8:28 AM | |
Posts: 8946 Rating:
|
Yes, the size of FC/FB but not the size of DB. |
Follow us on