10/28/2010 8:25 PM | |
Posts: 18 Rating:
|
I have a backup and want to download another same model PLC CPU315-2 DP, but the project was developed for the {} and I want to download at {315-2AF02-0AB0}. In the hardware config, the exchange of CPU, but when trying to download the error message occurs, there is "unable copy the block" of FC 86, FC 130, FC 200, DB 200 and OB82. What is the possible problem? Here attached the project. AttachmentTeste.zip (90 Downloads) |
10/29/2010 1:57 PM | |
Posts: 18 Rating:
|
Following error messages: (D280) Error compiling block in S7-300 CPU Message: Download(294:23) According to the help button, I ran the proper procedures. |
Follow us on