3/10/2017 8:23 AM | |
Joined: 4/23/2015 Last visit: 10/21/2024 Posts: 38 Rating:
|
I have managed to create a list of alarms in TIA portal V13 for my HMI. The alarms come up on an alarm page using an alarm view control. If the requirements for the alarm disappear, i.e. in this example the motor isnt overloaded anymore, i cannot see how to clear the alarm from the list. I would like to be able to do it both using a reset button on the front page of my HMI and also with an input using a reset button.
Attachment1.zip (87 Downloads) |
Follow us on