9/28/2017 5:40 PM | |
Posts: 439 Rating: (108) |
Hello, One of my customer tried to install STEP 7-Micro/WIN V4.0 SP6 on Windows 7, the installation aborted because of incompatibility with OS. STEP 7-Micro/WIN V4.0 SP6 is compatible with Windows XP, Windows Vista and Windows 2000, but not with Windows 7. STEP 7-Micro/WIN V4.0 SP9 on the other hand is compatible with Windows 7. Don't try to install something less and try to upgrade to SP9. You need to have V4.0 SP9 directly. So, I tried to install V4.0 SP9 after the aborted installation of SP6, but always got an error related to an earlier version of STEP 7-Micro/WIN installed... remove first then restart installation. I could see STEP 7-Micro/WIN V4.0 SP6 in "Uninstall ofr change a program" in my Control panel, but was unable to uninstall it. I found the below FAQ and tried it, but still get the same error... How do you uninstall STEP 7 Micro/WIN V4.0 after an aborted installation?So I opened a support request and they gave me the perfect working solution below. Thought it would help somebody else, so here it is:
Hope it helps! Have a good day! Hugo AttachmentMicrowin GUID Numbers.doc (653 Downloads) |
Last edited by: HugoD at: 9/28/2017 5:40:47 PM |
|
This contribution was helpful to6 thankful Users |
Follow us on