Industry Online Support
Technical Forum
8/6/2010 9:47 AM | |
Joined: 7/28/2010 Last visit: 4/25/2023 Posts: 184 Rating:
|
Jeebs, 1) Is the source of the plc code the same for both PCs or each PC has the plc code saved on its hard disk separate from the other PC? 2) Do you have a backup from the project that you can retrieve and check? 3)What is the communication line between the PCs and PLCs? Profibus or Ethernet? Regards, Behnam www.sigmaprocess.ca |
Follow us on