2/23/2010 1:26 PM | |
Joined: 10/7/2005 Last visit: 12/11/2023 Posts: 2997 Rating:
|
Hello Aden the FAQ below will hopefully give you the answers you are seeking regarding ISO protocol: What properties, advantages and special features does the ISO protocol offer? Note that you'll find links to similar entries for the the other protocols (e.g. ISO on TCP, TCP, UDP, S7 protocl etc.) at the top of that page. One more thing, PROFINET is actually NOT a Siemens proprietary protocol for industrial Ethernet, but instead atermcoined by PI (Profibus International)for "Ethernet-based networking solution for automation" andit is also governed by PI. You can find out more about it at www.profibus.com. Last but not least, you can find plenty of application examples for comms implementation for the various protocols at the address below: Simatic Net Quickstart I hope this helps |
Cheers |
|
This contribution was helpful to
2 thankful Users |
Follow us on