Industry Online Support
Technical Forum
1/6/2008 12:06 PM | |
Joined: 4/6/2006 Last visit: 1/21/2019 Posts: 604 Rating:
|
Hello maulik, I think there are a couple interesting documentsfor you. To talk about cabling/connectors and which of those could be combined the most interesting document is the IKPI 2007. And then Chapter 2 for Ethernet/ProfiNet, Chapter 4 for ProfiBus and Chapter 6 for AS-interface. It's necessary that you pick the IKPI 2007 and NOT the IKPI 2007 news since the tables and overviews are not available in there. A complete overview of the available chapters n the IKPI 2007 and the IKPI 2007 News is available with the following link: Catalog IKPI (SIMATIC NET) And a lot of information about the protocols and stuff like that can be found here: SIMATIC NET Twisted-Pair and Fiber-Optic Networks SIMATIC NET PROFIBUS Networks COMMUNICATION with SIMATIC Have fun reading. |
Best regards, |
|
1/8/2008 10:54 PM | |
Posts: 5822 Rating:
|
Hello, maybe I may add this Document too: Communication with SIMATIC S7 Best regards J_Bell |
1/10/2008 12:45 PM | |
Posts: 4 Rating:
|
Thank you very very much for your prompt reply. I will download the catalog and view it. |
Follow us on