2/23/2022 1:22 PM | |
Posts: 1 Rating:
|
Hello, I'm learning to use the library LPallPatt 109800960 I was trying to made a pallett with a brick pattern and i saw a strange result but i'm not sure that this behavior is normal With the application example I configure the generator following the parameters that you can see in parameters screenshot I configure the pattern mode " two block" with a mirorring on the Y axis at the center of the palett. I observe a difference between the odd layer and the even which is pretty logic because because i have a difference threw the Y axis However if keep the same settings and change the mirroring to X axis. Then the generator create exactly the same palett than with the Y axis. But normaly there is no difference with the X mirror. The odd and the even have to be the same but the generator create the same palett as with Y axis mode. Do you think that it's normal? |
Last edited by: Jen_Moderator at: 02/23/2022 14:16:49Optimized link. |
|
2/23/2022 6:22 PM | |
Joined: 7/7/2010 Last visit: 2/7/2025 Posts: 15619 Rating:
|
If you have a true cubic pallet layout, x-axis and y-axis mirroring should function correctly automatically. For a rectangular "cubic" pallet layout, the X and Y axis mirroring will be constrained in one axis - apparently that is the Y-axis on your sample pallet layout. Check the documentation (again) for what it can and cannot do, and then try to organize the pallets according to that.
|
science guy |
|
Follow us on