4/29/2021 3:03 PM | |
Joined: 1/25/2021 Last visit: 10/29/2023 Posts: 19 Rating:
|
This is trend from the same project but run on simulation and accessed through a browser. Comparing Side by Side. Left is panel, right is simulation I have realized that if I set my unified panel timezone to UTC 0, it works correctly. However if I set a time zone of UTC +7, the trend will not to function correctly. It seems that the trend time axis always starts at UTC 0, hence only present value can be seen. Is there a way to solve this? AttachmentFiles.zip (610 Downloads) |
Last edited by: casewhen at: 04/29/2021 15:20:04Last edited by: casewhen at: 04/29/2021 17:19:21Last edited by: Jen_Moderator at: 04/30/2021 08:38:59Removed link and added files as an attachment. |
|
4/30/2021 7:54 AM | |
Joined: 3/3/2021 Last visit: 11/12/2024 Posts: 271 Rating:
|
Hello Casewhen, please try to set the Timezone Property of the Trend Control: WinCC Unified V16: set the time zone property of the controls - YouTube If that does not help please also try to update the Panel to the newest Firmware: https://support.industry.siemens.com/cs/ww/de/view/109746530 I had some Issue with the Control and this was fixed by updating the firmware. Best Regards, Fred |
Last edited by: Jen_Moderator at: 04/30/2021 08:39:46Embedded video. |
|
4/30/2021 9:37 AM | |
Joined: 1/25/2021 Last visit: 10/29/2023 Posts: 19 Rating:
|
Hello Fred, I have just updated to MTP Firmware v16.0.5 but it still the same. I have also adjusted the time-zone accordingly, but it seems that the trend graph start plot always is UTC, hence the straight line shown in my original posting.
|
Follow us on