3/19/2025 10:38 AM | |
Joined: 5/6/2022 Last visit: 4/21/2025 Posts: 587 Rating:
|
Hi megaball, Regarding the tag limit, please note that the compilation of the project takes into account all elements of UDTs, Arrays and Structs which have to be less than 8,000 (soft limit) or 16,000 (hard limit) respectively: In principle, it is generally recommended to stay within the system limits, since full functionality of the system cannot be guaranteed. However, if you do not have any problems with the operation of the panel that you are saturating it, you can work without any problems. As for optimization, there is no documentation as such to be able to offer you some examples of best practice, you would have to review the dimensions of the project before doing a project to be able to review which Siemens equipment is the most suitable for your case. I don't know if anyone in this regard will be able to help you. Best regards!
|
If this Information really helps, you could use the Rate function |
|
Follow us on