11/17/2023 3:58 PM | |
Joined: 7/19/2022 Last visit: 1/13/2025 Posts: 432 Rating: (71) |
Hello K_Ohjus, According to the V18 GMP manual, it does generate a checksum for each entry: |
If this Information really helps, you could use the Rate function |
|
11/20/2023 5:10 AM | |
Joined: 3/5/2017 Last visit: 1/13/2025 Posts: 779 Rating: (129) |
Yes, Audit trail function works like it should, but only locally. After export there are no way to check file integrity. Statement below was not completely true last time I tested.
Yes, one can generate Audit reports and check integrity locally. What cannot be done is an export of whole database (preferred way) or export csv which integrity could be verified e.g. with Simatic Audit Viewer. If this has changed, that would be great.
|
- Trying is the first step towards failure. |
|
Follow us on