3/12/2024 9:09 AM | |
Joined: 8/3/2009 Last visit: 4/29/2025 Posts: 15369 Rating:
|
Hello AutoGen_7664921 Check if it works also with IP address instead of the PC name. Is the Webservercertificate installed on this PC and on the Office PC (if its another PC)? The Runtime has to be in run. Is the Username/PW active in the Project (loaded and usable?) check also the basics:
https://support.industry.siemens.com/cs/de/en/view/109821887 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on