2/5/2025 8:50 AM | |
Joined: 9/4/2018 Last visit: 3/17/2025 Posts: 7 Rating:
|
I'm currently testing this out on V20. Is it possible to use a color palette that you referenced in a faceplate type, in a script of this faceplate? I can do it with 'global' color palettes that are set up in the runtime settings of the device via the HMIRuntime.Resources.Colors(...) instruction. But I would prefer a unique color palette that is only used in certain faceplates. Is there a similar instruction like Faceplate.Resources.Colors(...)? I don't find any at the moment. Thanks in advance. ------------------------------------------------------------------------------------------ |
Last edited by: GSIM at: 02/05/2025 08:51:51Last edited by: Moderator_Lan at: 02/05/2025 09:22:20New subject after splitting |
|
2/6/2025 8:49 AM | |
Joined: 5/29/2024 Last visit: 3/18/2025 Posts: 101 Rating:
|
Hi GSIM! In the following link of the V20 manual you can find some indications: -> Generating a color palette as a type (RT Unified) Hope it helps! |
If this Information really helps, you could use the Rate function |
|
Follow us on