6/20/2016 4:11 AM | |
Posts: 4 Rating:
|
Hello, Could you help me to investigate how to connect between UniOP CP 10G-04-0045 and CPU 314 product via MPI standard via CA128 cable. Thank you so much AttachmentConnecting UniOP to Simatic S7 MPI.pdf (300 Downloads) |
6/20/2016 6:16 AM | |
Joined: 1/21/2013 Last visit: 11/20/2024 Posts: 4620 Rating:
|
Dear BaHoCa, Why? What problem you have? UniOP AUX Port to MPI Port / ADP-0001 MPI adapter to MPI Port Notes In case the panel is terminal node of the MPI network is necessary to use terminating resistors as shown in Figure 2. The Bus Connector 6ES7972-0BB20-0XA0 can be used for the PLC connector in order to provide the additional connection to the programming unit. Have you tried with Profibus cable and respective connector with terminating resistor? RS485 bus connector - Industry Mall - Siemens WW |
Last edited by: Ste39 at: 6/20/2016 6:17:24 AMLast edited by: Ste39 at: 6/20/2016 6:19:03 AM |
|
This contribution was helpful to
1 thankful Users |
6/27/2016 3:23 AM | |
Posts: 4 Rating:
|
Dear Sirs The cable is 03 meters. And I've tried for terminator on for two side but it did not work. May be it depends on the Firmware? |
Follow us on