6/24/2016 8:37 AM | |
Joined: 7/9/2015 Last visit: 3/24/2025 Posts: 4207 Rating:
|
Hi, here are some example applications about PUT/GET: Application for the "PUT" and "GET" Function Blocks of the S7 Communication
How do you program the function blocks FB14 "GET" and FB15 "PUT" in the S7 program of the S7-300 in order to transfer more than 160 bytes of data?Regards, Towome |
|
|
7/7/2016 5:32 PM | |
Posts: 9 Rating:
|
Myst, 1) You're rigth! 25 means the job is processing! So, the connection was good! 2) I was able to send data to S7-400 3) The length data configured in the GET and PUT blocks wasn't compatible. So, after I changed it, the unspecified S7 connection has worked very well! So, next week I will do it in the field project. Thank you all for your attention. See attached some pictures of the configured system. I did a program using the tutorial: https://support.industry.siemens.com/cs/document/18610307/how-do-you-program-communication-blocks-fb14-get-and-fb15-put-for-data-exchange-in-the-s7-program-of-an-s7-300-cpu?dti=0&lc=en-DE And I implemented the counter to see if the DONE signal of GET block were going to 1. For the next test, I will use the link of Towome about data transfer of more than 160 bytes using GET and PUT. Oshun Attachmentimages.zip (357 Downloads) |
Follow us on