Industry Online Support
Technical Forum
11/17/2012 10:43 AM | |
Joined: 8/31/2010 Last visit: 2/3/2023 Posts: 1498 Rating:
|
Hello MarceloSCS, There is no workaround in this case, as both these products are not supported by TIA Portal. In general moduleswhich were actively marketedsince2008 is supported in TIA Portal*. * - Still there are exceptions for this statement ways of checking products compatibility with TIA Portal is using - TIA Portal Readiness Check Tool(the enclosed document is generated by this tool only) or refering this FAQ - Which devices and modules are supported by STEP 7 Professional V11 and WinCC Professional V11? whichever of the above is latest. Ofcourse you can check in the Hardware Catalog of TIA Portal directly to check if a product is supported or not. AttachmentE:\SM 321 and SM 322.pdf (212 Downloads) |
Last edited by: Ganes10 at: 11/17/2012 10:45 AMLike it? Rate it! |
|
This contribution was helpful to
3 thankful Users |
Follow us on