Industry Online Support
Technical Forum
4/15/2014 9:14 AM | |
Joined: 11/14/2013 Last visit: 5/21/2024 Posts: 15 Rating: (0) |
Hello, My CPU 1511-1PN just arrived and it came with firmware versión V1.5. However, in my TIA Portal V12 SP1 I only have firmware V1.0 and V1.1. I stablish the connection with the CPU but when it starts uploading I get an error and I think it is because of this firmware mismatch. Could someone tell me how to update the catalog for S7-1500 so I have firmware V1.5 avaliable? I already installed the HSP of this link: https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&objId=72341852&nodeid0=28919804&load=content&subtype=133100&lang=en&siteid=cseus&aktprim=0&objaction=csview&extranet=standard&viewreg=WW I also installed the update 4 for TIA Portal V12 SP1. Still V1.5 does not appear in the catalog. Could someone help me? This shouldn't be so hard, I feel I am struggling too much with this. Thanks! |
4/15/2014 3:57 PM | |
Joined: 11/14/2013 Last visit: 5/21/2024 Posts: 15 Rating: (0) |
Then I will have to downgrade the firmware versión since V13 doesn't work on XP. I hopedowngrade is posible. |