3/31/2017 9:50 PM | |
Joined: 11/29/2011 Last visit: 2/4/2025 Posts: 1362 Rating:
|
Hi, Assuming you have a CP in your station. Time synchronization - Time synchronization in the automation environment |
- What you read here, please check with manuals and your requirements. |
|
4/3/2017 9:01 AM | |
Joined: 6/28/2016 Last visit: 3/11/2025 Posts: 44 Rating:
|
Hi Thank for the FAQ links My hardware is HMI= IPC277E 19'' Touch PN/IE and PLC=CPU 315-2 PN/DP What i don't understand is if with IPC277E, and Wincc V13 Runtime advanced, i can use the same method for synchronization like if PC is a HMI panel, or if i have to use a different strategy. According FAQ links, this is the method i try to use https://support.industry.siemens.com/cs/document/69864408/clock-synchronization-between-a-hmi-operator-panel-and-a-simatic-plc?lc=en-ww With area pointer Date/Time. In the list of devices, on HMI Operator devices, i can see SIMATC RT Advanced. That means the method is valid for synchronize the date/time of my IPC277E? I try to do it but seem the method don't work. Which method is suitable for date time synchronization for PC and Wincc Runtime advanced? |
Follow us on