10/1/2021 4:29 AM | |
Joined: 12/18/2014 Last visit: 3/20/2025 Posts: 34915 Rating:
|
Updates for SIMATIC WinCC Unified PC V17Updates for SIMATIC WinCC Unified PC RT V17 - 10/2021 Update WinCC Unified PC Runtime (07/2021) This update contains improvements regarding stability and performance of WinCC Unified PC Runtime. As already mentioned in the delivery release of WinCC Unified V17, for the operation of the Plant Intelligence optionPerformance Insight with a "File based Logging" this update of WinCC Unified PC on the RT Station is required. |
This contribution was helpful to
1 thankful Users |
Follow us on