4/27/2016 2:05 PM | |
Posts: 310 Rating: (18) |
Dear Christoph, I have Installed Wincc Basic ., Now how can i Update Wincc V13 to Professional . It Is possible to do . Or else i want to update Wincc v13 Sp1 ..?? Regards, Arasan.. ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 4/27/2016 2:38:55 PMNew subject after splitting |
|
4/27/2016 2:20 PM | |
Joined: 5/12/2006 Last visit: 1/17/2025 Posts: 22497 Rating: (3044)
|
Hello, WinCC V13 SP1 contains a Package Step7 Basic, which is default installed with the WinCC. So if you don't need the WinCC Professional or Advanced Featuresets (Other Panels, HMI RT support ...) then you must not update the WinCC Package. So you must only installed Step7 Professional V13 SP1 (Order Code 6ES7810-5CC11-0YA5). https://support.industry.siemens.com/cs/ww/en/view/106448872 Regards |
This contribution was helpful to1 thankful Users |
Follow us on