Industry Online Support
Technical Forum
10/1/2009 9:28 AM | |
Joined: 10/19/2005 Last visit: 11/30/2020 Posts: 1611 Rating:
|
Hi, the last Version from flexible are 2008 SP1 HF2 I mean that you should have the basic panels with flexible 2008 (but i am not sure if some basic panels comes with the SP1 for flexible 2008) SP1 -> http://support.automation.siemens.com/WW/view/en/34778772 HF2 -> http://support.automation.siemens.com/WW/view/en/36540041 If you use the SP1, then you need new images for the panels! I have make a screen shot from "my" flexible devices.(as Info) regards, |
10/8/2009 1:28 PM | |
Joined: 10/19/2005 Last visit: 11/30/2020 Posts: 1611 Rating:
|
Hi, this FAQ could be interesting for you. -> http://support.automation.siemens.com/WW/view/en/28531852 I use a VM-Ware and its works good. The only Problem are, that my CP5512 did notwork with the VM-Ware. Downloads are only be possible with "Ethernet". |
10/15/2009 7:18 PM | |
Posts: 11 Rating:
|
Yes I guess that I will use the VM-ware since all our updates are through TCP/IP. Thank you for all the help. Danath |
Follow us on