10/4/2007 11:48 AM | |
Posts: 1776 Rating: (95)
|
Hi, have you checked the readme? So I know between WinCC V6.0 SP3 and SP4 also a SP for SQL SP have to be installed. In WinCC 6.0 SP3 is SQL SP3 and in WinCC V6.0 SP4 is SQL SP4. See also http://support.automation.siemens.com/WW/view/en/22450372 The Runtime datas should not be loosed after this update, but save your project before you update. Or better create an Image of your installation for a fast way back, if something is happened. Godd luck April |
Follow us on