10/25/2021 6:04 PM | |
Posts: 257 Rating:
|
Hello SIOS-Forum-Community, We often receive questions about how to upgrade the licences of an existing Server/Client System in WinCC Professional.Below, an example of a configuration is described. Initial situation: Server/Client system (WinCC Professional V15.1) consisting of the following licences: - "SIMATIC WinCC Server for Runtime Professional" (Server). - "SIMATIC WinCC RT Professional, 4096 Power Tags V15.1" (Server) - "SIMATIC WinCC Client for Runtime Professional V15.1" (Client). Target: Upgrade existing Server/Client system to WinCC Professional V16. Solution:
Result (after upgrading the licences): Server/Client system (WinCC Professional V16) consisting of the following licences: - "SIMATIC WinCC Server for Runtime Professional" (Server). - "SIMATIC WinCC RT Professional, 4096 Power Tags V16" (Server) - "SIMATIC WinCC Client for Runtime Professional V16" (Client) In the delivery release of WinCC V16 there is an Excel file in which the order data of the WinCC licences are clearly summarised (see screenshot). https://support.industry.siemens.com/cs/ww/en/view/109771219 Further information can be found at the Siemens Industry Mall. - SIMATIC WinCC (TIA Portal) Options -> WinCC Server / WinCC Client - SIMATIC WinCC (TIA Portal) Runtime -> WinCC Runtime Professional Best regards, SIMATIC International Technical Support Hub. |
Follow us on