1/23/2024 11:45 AM | |
Joined: 7/19/2022 Last visit: 12/26/2024 Posts: 431 Rating: (71) |
Hello robbie c, Migration should not cause problems. The details of the migration are indicated in the V19 manual: SIMATIC STEP 7 Basic/Professional V19 and SIMATIC WinCC V19 starting on page 489. No specific issue to take into account is specified. Before performing the migration, it may be advisable to do a complete compilation to regenerate the project and then migrate it. |
If this Information really helps, you could use the Rate function |
|
Follow us on